AXIS#.SAFEPARAM.STO​.RESTARTACKMODE

Description

Indicates whether the Safe Torque Off (STO) will automatically reset or requires a manual reset using safe input or FSoE. In Automatic Restart mode, when the STO input clears, the STO automatically restarts and the drive is enabled. In Manual Restart mode, when the STO input clears, the STO remains active until the configured input triggers the STO to restart. See "AXIS#.SAFEPARAM.STO​.RESTARTACKSOURCE").

Value Description

0

Automatic Restart (default)

1

Manual Restart

 

Parameters Editor screen with Restart Acknowledge Behavior circled.

Context

For complete STO information refer to STO (Safe Torque Off).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-01-02-000

General Information

Type

Read/Write

Units

N/A

Range

0 (Automatic Restart)
1 (Manual Restart)

Default Value

0 (Automatic Restart)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.STO.RESTARTACKMODE

3152h

04h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.STO.RESTARTACKMODE

3252h

04h

Unsigned8

-

-

Read/Write

No