Actions Table
Use the Actions view to setup tasks for the drive to perform based on selected sources and conditions. Up to 32 actions can be configured. Each action has a minimum of 32 elements, which may have additional requirements.
Actions Table Terminology Compared to PLC Terminology
Action Configuration Order
Input Signal Types
Input signals are either analog or digital. The AKD2G supports up to 12 digital inputs (DIN1-12) and 2 analog inputs (AIN1-2).
Input Signal Trigger Conditions
An Action Task is triggered when the source input signal meets the criteria of the selected condition.
Digital Input Triggers
Analog Input Triggers
See Also
Actions Table Example, Execution, & Errors | Actions View Reference Table