AOUT.CUTOFF

Description

AOUT.CUTOFF sets the cutoff frequency in Hz for a single-pole low-pass
filter on the Analog Output.

A value of 0 Hz will turn off the filter and will allow all frequencies to pass through.

The filter can be used with all modes of Analog Output.

General Information

Type

NV Parameter

Units

Hz

Range

0 to 10,000 Hz

Default Value

0 Hz

Data Type

Float

Start Version

M_01-04-01

Variants Supported

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3470h/6

M_01-04-01-000

Related Topics

Analog Output