AOUT.MODE

Description

AOUT.MODE sets the analog output functionality.

AOUT.MODE Description

0

User variable. The analog output signal is determined by the user (using AOUT.VALUEU).

1

Actual velocity. The analog signal describes the current velocity value (VL.FB).

2

Velocity error. The analog signal describes the velocity error value.

3

Velocity command. The analog signal describes the velocity command value.

4

Actual current. The analog signal describes the actual current value.

5

Current command. The analog signal describes the current command value.

6

Actual position. The analog signal describes the current position value.

7

Position error. The analog signal describes the position error value.

8

Triangle wave. The analog signal is a triangle wave (sawtooth pattern).

9

Debug mode. In this mode the user can define a drive variable to monitor via the analog output (AOUT.VALUEU).

10

Unfiltered Velocity (VL.FBUNFILTERED)

11

Filtered Velocity - 10Hz Lowpass (VL.FBFILTER)

12 SynqNet AnalogOut (automatically set while SynqNet cyclic)

Example

You can use AOUT.MODE and AOUT.VALUEU to configure an output signal as follows:

-->AOUT.MODE 0

-->AOUT.VALUEU 5

-->AOUT.VALUEU 4.33

General Information

Type

NV Parameter

Units

N/A

Range

0 to 12

SynqNet: 12

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

Variants Supported

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3470h/1

M_01-00-00-000

Related Topics

Analog Output