DRV.CMDSOURCE

Description

DRV.CMDSOURCE specifies the source of the command to the drive. DRV.OPMODE sets the operation mode to the relevant control loop.

DRV.CMDSOURCE values can be set as follows:

Value

Description

0

Service, TCP/IP command

1

Fieldbus command

2

Gearing command

3

Analog command

5 Program command

If DRV.CMDSOURCE is set to 5 then DRV.OPMODE must be set to 3.

DRV.CMDSOURCE can be changed while the drive is enabled or disabled. If you use the terminal to change the operation mode, then it is recommended that you disable the drive before changing the command source.


  • If you change DRV.CMDSOURCE from the terminal while the drive is enabled, the system may experience a step change in command.

Example

To set the command source to the TCP/IP channel and the operation mode to velocity:

-->DRV.CMDSOURCE 0
-->DRV.OPMODE 1

General Information

Type

NV Parameter

Units

N/A

Range

0 to 5

0 to 1

BASIC: 0, 3, 5

SynqNet: 0

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No

Related Topics

DRV.OPMODE