DRV.FAULTHIST

Description

DRV.FAULTHIST returns the last 50 faults that occurred in the drive. The faults are shown with their fault number (which matches the one displayed on the drive display) and a timestamp that indicates when they last occurred.

Issue a DRV.CLRFAULTHIST to clear this fault log.

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

2012h

2013h

M_01-00-00-000

Related Topics

DRV.FAULTS, DRV.CLRFAULTHIST