DRV.IPEAK

Description

DRV.IPEAK returns the drive peak rated current in Arms.

General Information

Type

R/O Parameter

Units

Arms

Range

N/A

Default Value

N/A

Data Type

Float

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

5084h /0

M_01-00-00-000

Related Topics

"Foldback"

DRV.ICONT