IL.FRICTION

Description

Position command derivative sign is multiplied by this value to be injected to the current command.


  • IL.FRICTION is active in Position and Velocity modes (DRV.OPMODE = 1, 2), but not active in Torque mode (DRV.OPMODE = 0).

General Information

Type

R/W Parameter

Units

A

Range

0 to the minimum of user positive current limit (IL.LIMITP) and motor peak current (MOTOR.IPEAK).IL.LIMITP

Default Value

0

Data Type

Float

See Also

IL.FF

Start Version

M_01-00-00-000

Variant Supported
AKD EtherCAT Yes
AKD-N Yes
AKD-N Yes
AKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3422h/0 M_01-00-00-000

Related Topics

"Current Loop"