IL.KBUSFF

Description

This parameter scales the feedforward term added by the fieldbus to the current command. The nominal feedforward value can be multiplied by this gain value.

This parameter is only used in the position mode (DRV.OPMODE = 2).

General Information

Type

NV Parameter

Units

NA

Range

0 to 2

Default Value

0

Data Type

Float

See Also

IL.FF, IL.BUSFF

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

50E2h/0

M_01-00-00-000

Related Topics

Current Loop