IL.MFOLDD
Description
IL.MFOLDD sets the maximum time allowed for the motor to remain at peak current before starting to fold towards the motor continuous current. When at motor peak current, IL.MFOLDD is the amount of time before the foldback algorithm starts to reduce the current.
General Information
|
Type |
R/O Parameter |
|
Units |
s |
|
Range |
0.1 to 2400 s |
|
Default Value |
10 s |
|
Data Type |
Float |
|
See Also |
Foldback |
|
Start Version |
M_01-00-00-000 |
| Variant | Supported |
|---|---|
| MKD EtherCAT | Yes |
| AKD-N | Yes |
| MKD-N | Yes |
| MKD-C | No |
Related Topics