MOTOR.ICONT

Description

This parameter is used to configure the motor continuous current.

General Information

Type

NV Parameter

Units

A

Range

0.1 to 500 A

Default Value

1.0 A

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

AKD BASIC Information

Type

R/W

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
358Eh/0 M_01-00-00-000

Related Topics

"Motor View"