MOTOR.KT

Description

This parameter is the torque constant of the motor in Nm/A.The value can be online checked according to the following equation:

Kt = 60 *√3 * Ui/( 2 * π* n)

Where:

Ui = induced voltage of the motor
n = actual rotor velocity

General Information

Type

NV Parameter

Units

Nm/A

Range

0.001 Nm/A to 1,000,000.000 Nm/A for rotary motors.

0.001 Nm/A to 1,000,000.000 N/A for linear motors.

Default Value

0.1 Nm/A

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3593h/0 M_01-00-00-000

Related Topics

"Motor View"