VBUS.UVMODE
Description
This parameter indicates undervoltage (UV) mode.
When VBUS.UVMODE - 0, an undervoltage fault is issued whenever the DC bus goes below the undervoltage threshold.
When VBUS.UVMODE = 1, an undervoltage fault is issued whenever the DC bus goes below the
under voltage threshold and the controller attempts to enable the drive (software or hardware enable).
General Information
|
Type |
N/V Parameter |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
| Variant | Supported |
|---|---|
| MKD EtherCAT | Yes |
| MKD-N | Yes |
| MKD-C | No |
| Index/Subindex | Object Start Version |
|---|---|
|
3617h/0 |
M_01-00-00-000 |
Related Topics
1 Regeneration