VL.LIMITP

Description

VL.LIMITP sets the velocity command positive limit.

If the input to the velocity loop is higher than VL.LIMITP, then the actual velocity command VL.CMD is limited by the value of VL.LIMITP.

General Information

Type

NV Parameter

Units

Depends on UNIT.VROTARY (pg 1) or UNIT.VLINEAR (pg 1)

Rotary: rpm, rps, deg/s, custom units/s, rad/s

Linear: counts/s, mm/s, µm/s, custom units/s

Range

Range may be limited by ECCN 3A225 Limitations for Induction Motors

Rotary:

0.000 to 15,000.000  rpm

0.000 to 250.000  rps

0.000 to 90,000.000 deg/s

0.000 to 1,250.000 custom units/s

0.000 to 1570.796 rad/s

Linear:

0.000 to 1,073,741,824,000.000 counts/s

0.000 to 250.000*MOTOR.PITCH mm/sec

0.000 to 250,000.000*MOTOR.PITCH µm/s

0.000 to 1,250.000 custom units/s

Default Value

Rotary:

3,000.000  rpm

50.000 rps

18,000.002 deg/s

250.000 (custom units)/s

314.159 rad/s

Linear:

0.050 counts/s

50.000*MOTOR.PITCH mm/sec

50,000.004*MOTOR.PITCH µm/sec

250.000 custom units/s

Data Type

Float

See Also

VL.LIMITN, VL.CMD

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3622h/0 M_01-00-00-000

Related Topics

Velocity Loop