FBD Comments

Comment text area can be entered anywhere in an FBD diagram.

  • Select the Insert Comment Text button in the FBD toolbar to insert a new comment area.
  • In this mode, the mouse is used to insert comment text areas anywhere in the diagram.
  • Click in the diagram and drag the text block to the desired position.
  • Double-click on the comments area to enter or change the attached text.

  • A hyperlink can be inserted In external files.
    Only TXT and BMP extensions are allowed.
    When the link is valid, the hyperlink is replaced with the file's content.

          

Figure 1: FBD Comments - Inserting Graphic