Select FBD Variables and Instances
![]()
Click this button or press <Esc> before any selection.
Double-click on the tag-name gray area.
These types of object must be linked to valid symbols:
|
Tool |
Button |
Description |
|---|---|---|
| Block |
|
For a function block, you must specify the name of a valid declared instance of the corresponding type. |
| Coil |
|
Must be attached to a declared Boolean variable. |
| Contact |
|
Must be attached to a declared Boolean variable. |
| Jump |
|
Must have the same name as its destination label. |
| Label |
|
Must have a name. The name must be unique within the diagram. |
| Variable |
|
Must be attached to a declared variable. Alternatively, a variable box may contain the text of a valid constant expression. |
Symbols of variables and instances are selected using a variable list, that can be used as the variable editor.
- Enter a symbol or constant expression in the Edit box and click OK.
- Select a name in the list of declared objects or
click the Create button to declare a new variable.