FFLD Jumps and RETURN

A jump to a label branches the execution of the program after the specified label.

  • In the FFLD Language, the >> symbol (followed by the target label name) is used as a coil at the end of a rung.

       

  • The jump is performed only if the rung state on input is TRUE.
    • The destination label must be specified on a network of the same program.
    • To specify the destination, double-click the cell to display a drop-down menu that lists all the available labels.

  • The special <RETURN> destination specifies a jump to the end of the program.