AS-interface Functions
|
Function |
Description |
|---|---|
|
ASiReadPI |
Read actual parameters of an AS-i slave. |
|
ASiReadPP |
Read permanent parameters of an AS-i slave. |
|
ASiSendParam |
Send parameters to an AS-i slave. |
|
ASiStorePI |
Store actual parameters as permanent parameters. |
|
ASiWritePP |
Write permanent parameters of an AS-i slave. |
-
-
AS-i networking may be not available on some targets.
See the OEM instructions for more information.
Interface
Params := ASiReadPP (Master, Slave);
bOK := ASiWritePP (Master, Slave, Params);
bOK := ASiSendParam (Master, Slave, Params);
Params := ASiReadPI (Master, Slave);
bOK := ASiStorePI (Master);
Arguments
Master : DINT Index of the AS-i master (1..N) such as shown in configuration.
Slave : DINT Address of the AS-i slave (1..32 / 33..63).
Params : DINT Value of AS-i parameters.
bOK : BOOL TRUE if successful.