Bookmarks

Bookmarks are used for navigating in a document.

  • Insert bookmarks anywhere in a document.
    • Use them to jump from one bookmark to another with a single command for browsing the document.
  • Bookmarks are supported in all program editors plus the Variable editor.

These are the available commands for using bookmarks:

Command

Description

Ctrl + F2

Toggle the bookmark at the current position.

Shift + F2

Go to the next bookmark.

According to the type of document, the possible locations for a bookmark are:

  • In the FBD editor, a bookmark is placed on any FBD object (not on a line).
  • In the FFLD editor, a bookmark is placed on a rung header.
  • In the SFC editor, a bookmark is placed on an SFC symbol (step, transition, jump...).
  • In the text editor, a bookmark is placed on a line of text.
  • In the Variable editor, a bookmark is placed on any line of the grid (variable or group).

  • Bookmarks are valid only while the editing window is open.
    They are not stored in the document when the window is closed.