eipAdapter
Function Block - Provides information about the current state of the Scanner connection.
Inputs
-
- There are no Inputs for this function / function block.
It automatically refers to the adapter in the project.
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Run |
BOOL |
FALSE, TRUE |
N/A |
TRUE, if the EIP stack is running. |
|
IOcnx |
BOOL |
FALSE, TRUE |
N/A |
TRUE, if an I/O connection is established with the Scanner. |
Remarks
- This function block is used in a program on the Adapter side.
- The servers (adapters) accessed by this block must be configured in the EtherNet/IP Scanner fieldbus configuration.
- Only one explicit message (read or write) can be sent at one time to the same server.
- If another message is pending you receive the error report 3 (busy) after calling the block to start a new exchange.
- Consider SerializeIn and SerializeOut functions for extracting data from the read buffer.
Example
Inst_eipAdapter(); // read the EtherNet/IP adapter status
EIP_running := Inst_eipAdapter.Run; // is it running?
EIP_connected := Inst_eipAdapter.IOCnx; // and connected?
See Also