eipRestartCnx
This function/function block was added in KAS v4.03.
Function - The EIP I/O connection is restarted when this function is called.
Example: ForwardClose and ForwardOpen requests are sent to the specified EIP adapter IP address. RJ45
-
- This function should be only called under certain conditions (e.g., IF statements, etc.).
It should not be called every cycle.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IP |
STRING |
No range |
N/A |
No default |
IP address of the Ethernet I/P adapter device. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
FALSE, TRUE |
N/A |
Result of the function call. If FALSE, the specified IP address in the Input is incorrect. |
Figure 1: eipRestartCnx
Remarks
None
FBD Language Example
Not available.
FFLD Language Example
IL Language Example
Not available.
ST Language Example
IF bRestartEipCnx THEN
bOK := EipRestartCnx( '10.50.66.109');
bRestartEipCnx := FALSE;
END_IF;