FB_ElapseTime
Function Block - Keeps track of the time (oTotalOnTime) a Boolean input variable is on.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
iEN00 |
BOOL |
FALSE, TRUE |
N/A |
FALSE |
Enable for the block. |
|
iVariable |
BOOL |
FALSE, TRUE |
N/A |
FALSE |
The variable to be tracked. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
FALSE, TRUE |
N/A |
Function block is OK. This output follows the state on iEN00 input. |
|
oTotalOnTime |
TIME |
0ms - 24hr |
ms |
The amount of time the iVariable is turned on. |
|
oInProcess |
BOOL |
FALSE, TRUE |
N/A |
The state of the block’s execution whether or not it is still keeping track of time. |
|
oDone |
BOOL |
FALSE, TRUE |
N/A |
The state of the block’s execution whether or not it is completed. |
Remarks
- Once the iEN00 enable input is high, the Kollmorgen UDFB keeps track of the total time iVariable is on.
- If iVariable changes to an off state while iEN00 is on, the oTotalOnTime stops.
- oTotalOnTime will start to add again once iVariable changes state to high.
- As long as the iEN00 input is on, iVariable can change states many times.
- The oTotalOnTime will reflect only the total time that iVariable has been on.
- While iVariable is still TRUE, oInProcess is also TRUE and oDone is FALSE.
- Once iVariable is FALSE, oInProcess is FALSE and oDone is TRUE.
- If the iEN00 input goes off, oTotalOnTime stops counting and the Kollmorgen UDFB execution stops.
- To restart the timer turn iEN00 on again.
- This resets oTotalOnTime to zero and counting begins once iVariable is also on.
Figure 1: FB_ElapseTime
Figure 2: MFB_ElapseTime – Time Diagram
Usage
- Enable the block by setting iEN00 to TRUE
- Either manually set iVariable to TRUE or have the application set this variable to TRUE
- Once oDone returns TRUE, read the oTotalOnTime to find out how long iVariable was on.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Keep track of total time that IncremementTimer variable is TRUE while EnableTimer variable is true
//Timer will be reset when EnableTimer variable is false
Inst_FB_ElapseTime( EnableTimer, IncrementTimer );
TotalOnTime := Inst_FB_ElapseTime.oTotalOnTime;