MC_GrpReadActAcc
Function Block - Reads the actual acceleration of the group and the axes in the group.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Enable |
BOOL |
FALSE, TRUE |
N/A |
No default |
If TRUE, this function block reads the current actual acceleration of the group and the axes in the group. |
||||||||
|
AxesGroup |
No range |
N/A |
No default |
The axes group the actual acceleration is read from. |
|||||||||
|
CoordSystem |
SINT |
Enumerated |
N/A |
No default |
The coordinate system used when reading the actual acceleration. One of these enumeration values:
|
||||||||
|
Acceleration |
LREAL[ ] |
Dimension: The number of axes in the AxesGroup. No range |
User unit/sec2 |
No default |
An array where the acceleration data is written.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Valid |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the accelerations have been read without error. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
INT |
Enumerated |
N/A |
Indicates the error if Error output is TRUE. |
|
PathAcceleration |
LREAL |
No range |
User unit/sec2 |
The current measured path acceleration of the group. This is measured by taking the square root of the sum of the squared accelerations of each axis. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller.
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- See Function Blocks - General Rules about how inputs and outputs work.
- The MC_GrpReadActAcc function block fills the array specified by the Acceleration argument with the actual acceleration of the system in the coordinate system specified by the
CoordSystemargument.- The measured path acceleration is calculated and reported via the PathAcceleration output.
- This function or function block does not generate any motion.
-
-
- The actual acceleration is smoothed over the last 10 samples.
This reduces the error in acceleration estimation but introduces a small amount of phase delay in the reported accelerations. - Only the ACS coordinate system is supported.
See Coordinate Systems.
- The actual acceleration is smoothed over the last 10 samples.
- There is a one-to-one correspondence between the axes in AxesGroup and the acceleration values in the Acceleration array.
- If an index in AxesGroup is unassigned, the acceleration value for that array element in the Acceleration array is 0 (zero).
- If the element does contain an axis, the Acceleration element is filled with the current actual acceleration for that axis.
Figure 1: MC_GrpReadActAcc
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Inst_MC_GrpReadActAcc( DoRead, Group, CoordSys, AccList );
See Also