MC_MoveDirRel
Function Block - Commands movement of an axes group to a relative position regardless of path.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, request to perform a direct relative move. |
||||||||
|
AxesGroup |
No range |
N/A |
No default |
Reference to an axes group. |
|||||||||
|
Distance |
LREAL[ ] |
Dimension: The number of axes in the AxesGroup. No range |
User units |
No default |
An array containing the distance for each axis in the group. |
||||||||
|
CoordSystem |
SINT |
Enumerated |
N/A |
No default |
The coordinate system used when commanding the direct relative move.
One of these enumeration values:
|
||||||||
|
BufferMode |
SINT |
Enumerated |
N/A |
No default |
These are the valid buffer modes for this function block:
See Buffer Modes. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Busy |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the function block is executing. |
|
Active |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the function block is controlling motion. |
|
CommandAborted |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command was aborted by another function block. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
INT |
Enumerated |
N/A |
Indicates the error if Error output is TRUE. |
Remarks
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- See Function Blocks - General Rules about how inputs and outputs work.
- When all motion has completed successfully, the axes group state is GroupStandby.
- MC_MoveDirRel commands a movement of an axes group to a relative position in the specified coordinate system regardless of how (on which path) the target position is reached.
-
-
- An error is returned if the group is in the GroupDisabled state.
- This function block does not have its own Acceleration, Deceleration, Velocity, and Jerk arguments.
- These are set using MC_AxisSetDefaults.
- The maximum number of axes is set by the MaxNumberOfAxes input set in the MC_CreateAxesGrp function block.
-
-
- Circular motion is only supported for axes groups with only two attached axes.
Figure 1: MC_MoveDirRel
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Inst_MC_MoveDirRel(ExecuteMove, Group1_Ref, DistanceList, , CS_ACS, BM_ABORTING);
See Also