MC_MoveLinAbs
Function Block - Commands interpolated linear movement on an axes group to the specified absolute positions.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, request to perform a linear absolute move. |
||||||||
|
AxesGroup |
No range |
N/A |
No default |
The axis group that performs the linear absolute move. |
|||||||||
|
Position |
LREAL[ ] |
Dimension: 1 to 256 No range |
User units |
No default |
Array of absolute end positions for each axis in the group. |
||||||||
|
Velocity |
LREAL |
0 < Velocity < (20 * Acceleration) and |
User unit/sec |
No default |
Maximum velocity of the defined path. |
||||||||
|
Acceleration |
LREAL |
Acceleration > (Velocity / 20) |
User unit/sec2 |
No default |
Maximum acceleration. |
||||||||
|
Deceleration |
LREAL |
Deceleration > (Velocity / 20) |
User unit/sec2 |
No default |
Maximum deceleration. |
||||||||
|
Jerk |
LREAL |
Trapezoidal velocity profiles: S-Curve velocity profiles: |
User unit/sec3 |
No default |
Maximum jerk. |
||||||||
|
CoordSystem |
SINT |
Enumerated |
N/A |
No default |
The coordinate system used when commanding the linear absolute move.
One of these enumeration values:
|
||||||||
|
BufferMode |
SINT |
Enumerated |
N/A |
No default |
Defines the chronological sequence of the function block relative to the previous block.
|
||||||||
|
TransitionMode |
SINT |
Enumerated |
N/A |
No default |
Coupled with the TransitionParameter, this input defines the shape and dynamics of the inserted contour to connect the current motion with the next motion in the queue.
One of these enumeration values:
|
||||||||
|
TransitionParameter |
LREAL[ ] |
Dimension: 1 to N No range |
N/A |
No default |
This array is dependent on the specified TransitionMode.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Busy |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the function block is executing. |
|
Active |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the function block is controlling motion. |
|
CommandAborted |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command was aborted by another function block. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
INT |
Enumerated |
N/A |
Indicates the error if Error output is TRUE. |
Remarks
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- When all motion has completed successfully, the axes group state is GroupStandby.
- MC_MoveLinAbs commands interpolated linear movement on an axes group to the specified absolute positions in the coordinate system as specified by the CoordSystem argument.
- The dimensionality of the move is determined by the number of axes mapped to the group.
-
-
- An error is returned if the group is in the GroupDisabled state.
- The maximum number of axes is set by the MaxNumberOfAxes input set in the MC_CreateAxesGrp function block.
-
-
- Circular motion is only supported for axes groups with only two attached axes.
Figure 1: MC_MoveLinAbs
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* Inst_MC_MoveLinAbsST example *) Inst_MC_MoveLinAbs( ExecuteLinearMove, Group1_Ref, PositionList, Velocity, Acceleration, Deceleration, Jerk, CoordSystem, BufferMode, TransitionMode, TransitionParams );
See Also