MC_GrpSetPos
Function Block - Sets the axis command position for all of the axes in an axes group to the positions specified in the Position input.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, request to set the position of the group. |
||||||||
|
AxesGroup |
No range |
N/A |
No default |
The axis group to set the positions. |
|||||||||
|
Position[] |
LREAL |
0, Number of axes in group-1 |
N/A |
No default |
An array containing the position for each axis in the group.
|
||||||||
|
Relative |
BOOL |
FALSE, TRUE |
N/A |
No default |
Request to set position:
|
||||||||
|
CoordSystem |
SINT |
Enumerated |
N/A |
No default |
The coordinate system used when setting the positions.
One of these enumeration values:
|
||||||||
|
BufferMode |
SINT |
0 to 0 |
N/A |
No default |
Unused. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Busy |
BOOL |
FALSE, TRUE |
N/A |
Returns FALSE. |
|
CommandAborted |
BOOL |
FALSE, TRUE |
N/A |
Returns FALSE. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
INT |
Enumerated |
N/A |
Indicates the error if the Error output is set to TRUE. |
Remarks
-
- This function block starts a motion-related action and stores data for calculations and error checking.
If using a dual-core controller, see Call Function Blocks Multiple Times in the Same Cycle.
- This function or function block does not generate any motion.
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- The axes group must be enabled and in Standby mode for MC_GrpSetPos to execute.
- If it is not, this FB returns an error and the axis positions remains unchanged.
- The command position is that returned by the FB MC_GrpReadCmdPos.
Figure 1: MC_GrpSetPos
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Inst_MC_GrpSetPos( DoSetPos, Group1, PositionArray, Relative, MC_COORDINATE_SYSTEM_ACS, 0 );
See Also