MC_ClearFaults
Function -
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
En |
BOOL |
FALSE, TRUE |
N/A |
No default |
Function enable - execute function. is this statement necessary? When TRUE, requests to clear the drive faults. |
|
Axis |
AXIS_REF |
1 to 256 |
N/A |
No default |
AXIS_REF.AXIS_NUM is the master axis number.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
FALSE, TRUE |
N/A |
Boolean output to indicate successful request.
|
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller.
- See Function Blocks - General Rules about how inputs and outputs work.
- The condition causing the drive fault has to be corrected before calling this function.
- If the fault condition still exists when this function is called, this function sends a request to the drive but the drive faults remain.
- This function does not reset axis errors.
- MC_ResetError is required to reset axis errors and possibly to re-enable or turn power on to the servo axis after the fault condition is cleared.
Usage
When there is a positive transition of the EN input, this function requests a Fault Reset of the Drive for the Axis defined in the axis input of this function.
Figure 1: MC_ClearFaults
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MC_ClearFaults ST example *)
MC_ClearFaults( Axis1); //clear drive faults for Axis 1
See Also