MLAddInit
Function - Initializes an Adder Pipe Block for use in a PLC Program with user-defined settings.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of a created Pipe Block. |
|
Ratio1 |
LREAL |
No range |
N/A |
No default |
Sets the Ratio value of the first entry of an Adder object. |
|
Offset1 |
LREAL |
No range |
N/A |
No default |
Sets the Offset value of the first entry of an Adder object. |
|
Ratio2 |
LREAL |
No range |
N/A |
No default |
Sets the Ratio value of the second entry of an Adder object. |
|
Offset2 |
LREAL |
No range |
N/A |
No default |
Sets the Offset value of the second entry of an Adder object. |
Outputs
Adder Block Output = Ratio1*Input1 + Offset1 + Ratio2*Input2 + Offset2
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE if the Adder Pipe Block is initialized. See Function - General Rules. |
Remarks
-
-
Adder objects are normally created in the Pipe Network using the graphical engine.
You do not have to add MLAddInit function blocks to their programs.
Parameters are entered directly in pop-up windows and the code is automatically added to the current project.
- Function block is automatically called if an Adder Block is added to the Pipe Network.
- User-defined settings are entered in the Pipe Blocks Properties screen.
- The Pipe Block is assigned ratios and offsets for both inputs.
- After an Adder block is initialized, the inputs need to be selected using the MLAddWriteInput function block or graphically using the Pipe Network.
Figure 1: MLAddInit
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Create and Initiate a Trigger object
MyAdder := MLBlkCreate( 'MyAdder', 'ADDER' );
MLAddInit( MyAdder, 1.0, 0.0, 1.0, 0.0 );
See Also