MLAxisReadGenStatus
Function - Returns the status of the internal generator of the axis.
The status of the Axis generator: acceleration, run, deceleration, change designation point, single step.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ID |
DINT |
No range |
N/A |
No default |
ID Name of the Axis block. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when the function successfully executes. See Function - General Rules. |
|
Default (.Q) |
DINT |
|
|
Shows the status of the internal generator based on the Internal Generator Status table. See Function - General Rules. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller.
Internal Generator Status
|
Status |
Description |
|---|---|
|
0 |
RUN mode (acceleration). |
|
1 |
RUNNING or STOPPED. |
|
2 |
MOVE: Changing move destination. |
|
3 |
MOVE: Changing move destination. |
|
4 |
MOVE: Acceleration. |
|
5 |
MOVE: Constant speed (travel speed). |
|
6 |
MOVE: Deceleration. |
|
7 |
MOVE: Single step (micro movement). |
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLAxisReadGenStatus(PipeNetwork.Axis1 ) ;
See Also