MLCompWriteRef
Function - Sets the reference position of a comparator block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of an initiated Comparator object. |
|
ThroughZero |
BOOL |
0, 1 |
N/A |
No default |
|
|
Reference |
LREAL |
No range |
User units |
No default |
New reference position to set in the selected Comparator object. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when function starts to execute. See Function - General Rules. |
Remarks
- The Transition Flag of a comparator object turns TRUE if the input position to the comparator is greater or equal to the reference.
- The Comparator Transition Flag stays TRUE until it is reset.
- If the input ThroughZero is set to TRUE, system must cross zero and then the reference position before the Transition Flag is set.
- If ThroughZero is FALSE, Transition Flag is set immediately if the input pipe position is greater then or equal to the Reference value.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Set the Comparator Reference value
MLCompWriteRef( PipeNetwork.MyComp , TRUE , 45 );
See Also