MLCNVInit
Function - Initializes a converter Pipe Block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of a created Pipe Block. |
|
Mode |
DINT |
1, 2 |
N/A |
No default |
Determines the type of input to the Converter Object.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE if the Convertor Pipe Block is initialized. See Function - General Rules. |
Remarks
- MLCNVInit is automatically called if a Convertor Block is added to the Pipe Network, with the input mode (position or speed) entered in the Pipe Blocks Properties screen.
- The Converter block changes the incoming flow of speed or position values to continuous position output with no periodicity.
-
-
Converter objects are normally created in the Pipe Network using the graphical engine.
You do not have to add MLCNVInit function blocks to their programs.
Parameters are entered directly in pop-up windows and the code is then automatically added to the current project.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
// Initiate a created convertor block named “CNV1”
CNV1 := MLBlkCreate( 'CNV1', 'CONVERTOR' );
MLCNVInit( CNV1, 1 );
See Also