MLMstInit
Function - Initializes a Master TMP generator block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of the Master Block. |
|
ModuloPosition |
LREAL |
No range |
User units |
No default |
Modulo Position for cyclic motion systems expressed in user logical units (Position Rollover Value). |
|
Period |
LREAL |
No range |
Cycles |
No default |
Sampling period of the generator expressed according to the update cycle. Example: 2.0 means the sampling is done once every 2 cycles. |
|
Speed |
LREAL |
No range |
User units |
No default |
Travel speed value expressed in user logical units per second.
|
|
Acceleration |
LREAL |
No range |
User unit/sec2 |
No default |
Acceleration value expressed in user logical units per second squared.
|
|
Deceleration |
LREAL |
No range |
User unit/sec2 |
No default |
Deceleration value expressed in user logical units per second squared.
|
|
InitialPosition |
LREAL |
No range |
User units |
No default |
Initial position value expressed in user logical units. Used only at the pipe activation to initialize the position starting point. |
|
Modulo |
BOOL |
FALSE, TRUE |
N/A |
No default |
The available modes are:
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when the function successfully executes. See Function - General Rules. |
Remarks
- This function is automatically created when the MLMaster Block is included in the Pipe Network Editor.
- Based on the parameters defined in the Master pipe block, the Inputs for this function are initialized by default.
- See example in the Figure 1.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Initialize a Master Pipe Block named “MASTER” to a Modulo of 360, motion generator sample period of 1,Speed of 1000.0, Accel and Decel of 10000.0, Initial position of 0.0,
MLMstInit( PipeNetwork.MASTER, 360.0, 1.0, 1000.0, 10000.0, 10000.0, 0.0, true );