MLSmpConECAT
Function - Connects a sampler block to the specified CoE object in a PDO.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID Name of the SMP function block in the Pipe Network. |
|
DeviceAddr |
INT |
No range |
N/A |
No default |
The EtherCAT address of the slave device.
|
|
Index |
UINT |
No range |
N/A |
No default |
The CoE index of the object to be connected with the Sampler block. |
|
SubIndex |
USINT |
No range |
N/A |
No default |
The CoE sub-index of the object to be connected with the Sampler block. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Function block is operational. See Function - General Rules. |
Remarks
- The CoE object must be included in a PDO for the specified EtherCAT device.
- Use any EtherCAT data source as input for the specified sampler block.
- If the device providing the CoE Object for the Sampler block is removed:
- The CoE object value becomes 0 (zero) if the EtherCAT device providing the CoE object for the Sampler block is removed using the ECATDeviceAction function block.
- The CoE object automatically connects to the sampler block when the device is reconnected to the EtherCAT network.
- This function can be programmed from within the Pipe Network block.
Right-click the block and click Properties.
Figure 1: MLSmpConECAT
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Connect a Sampler pipe block named “EncoderMaster” to an ECAT Index Object defined by variable “CoE_SubIndex” with the SubIndex defined by variable “CoE_SubIndex”, from a device with Ethercat Address defined by “ECAT_Addr”
MLSmpConECAT(PipeNetwork.EncoderMaster, ECAT_Addr, CoE_Index, CoE_SubIndex );
See Also