ApplyRecipeColumn
Function - Apply the values of a column from a recipe file.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
FILE |
STRING |
|
|
|
Path name of the recipe file (.CSV or .RCP). Must be a constant value. |
|
COL |
DINT |
|
|
|
Index of the column in the recipe (0 (zero) based). |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
|
|
|
Remarks
- The FILE input is a constant string expression specifying the path name of a valid .CSV or .RCP file.
- If no path is specified, the file is assumed to be located in the project folder.
- CSV files are created using Excel or Notepad.
- RCP files are created using an external recipe editor.
- In CSV files, the first line must contain column headers, and is ignored
during compiling.
- There is one variable per line.
- The first column contains the symbol of the variable.
- Other columns are values.
- If a cell is empty, it is assumed to be the same value as the previous (left
side) cell.
- If it is the first cell of a row, it is assumed to be null (0 or FALSE or empty string).
Example of CSV file with five variables and five set of values
comment lines here
TravelSpeed;100;200;300;400;500
MasterAbsPos;0;45;90;135;180
MasterDeltaPos;0;90;180;270;360
MachineSpeed;50;100;150;200;250
MachineState;0;0;1;1;2
-
-
For the CSV file to be valid, ensure the data are separated with semicolons (NOT commas).
Usage in an FFLD program where column 3 is selected.
Column 3 corresponds to column E in the Excel sheet because this parameter is 0 based.
Result displayed in the Dictionary when the application is running.
@COLNAME=Col3 Col4
@SIZECOL1=100
@SIZECOL2=100
@SIZECOL3=100
@SIZECOL4=100
bCommand
tPerio
bFast
Blink1
test_var
bOut
@EXPANDED=Blink1
-
-
Recipe files are read at compiling time and are embedded into the downloaded application code.
This implies that a modification performed in the recipe file after downloading is not taken into account by the application.
FBD Language Example
FFLD Language Example
- In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung is the result of the function.
- The function is executed only if ApplyRecipe is TRUE.
IL Language Example
Op1: LD 'MyFile.rcp'
ApplyRecipeColumn COL
ST OK
ST Language Example
OK := ApplyRecipeColumn ('MyFile.rcp', COL);