LIFO
Function Block - Manages a last in / first out list.
Inputs
|
Inputs |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BUFFER |
ANY |
|
|
|
Array for storing values. |
|
NEXTOUT |
ANY |
|
|
|
Value at the top of the stack. Updated after call. |
|
NEXTIN |
ANY |
|
|
|
Value to be pushed. |
|
POP |
BOOL |
|
|
|
Pop a new value on the rising edge. |
|
PUSH |
BOOL |
|
|
|
Push a new value on the rising edge. |
|
RST |
BOOL |
|
|
|
Reset the list. |
Outputs
|
Outputs |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
EMPTY |
BOOL |
|
|
TRUE if the list is empty. |
|
OFLO |
BOOL |
|
|
TRUE if the overflow is on a PUSH command. |
|
Count |
DINT |
|
|
Number of values in the list. |
|
pRead |
DINT |
|
|
Index in the buffer of the top of the stack. |
|
pWrite |
DINT |
|
|
Index in the buffer of the next push position. |
Remarks
- NEXTIN, NEXTOUT, and BUFFER must have the same data type.
- It cannot be a STRING.
- The NEXTOUT argument specifies a variable filled with the value at the top of the stack after the block is called.
- Values are stored in the BUFFER array.
- Data is never shifted or reset.
- Only read and write pointers and pushed values are updated.
- The maximum size of the stack is the dimension of the array.
- The first time an instance of the LIFO function block is called, that instance stores which array is passed to BUFFER.
- If a later call to the same instance passes a different array for the BUFFER argument, the call is considered invalid and no action is performed.
- The EMPTY output returns TRUE in this case.
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung is the PUSH input.
- The output rung is the EMPTY output.
IL Language Example
(* MyLIFO is a declared instance of LIFO function block *)
Op1: CAL MyLIFO (PUSH, POP, RST, NEXTIN, NEXTOUT, BUFFER)
FFLD MyLIFO.EMPTY
ST EMPTY
FFLD MyLIFO.OFLO
ST OFLO
FFLD MyLIFO.COUNT
ST COUNT
FFLD MyLIFO.PREAD
ST PREAD
FFLD MyLIFO.PWRITE
ST PWRITE
ST Language Example
(* MyLIFO is a declared instance of LIFO function block. *)
MyLIFO (PUSH, POP, RST, NEXTIN, NEXTOUT, BUFFER);
EMPTY := MyLIFO.EMPTY;
OFLO := MyLIFO.OFLO;
COUNT := MyLIFO.COUNT;
PREAD := MyLIFO.PREAD;
PWRITE := MyLIFO.PWRITE;
See Also