File Name Warning and Limitations
- File names in the controller's flash storage are case-sensitive.
- The SD card or USB flash drive (FAT16 or FAT32) are not case-sensitive.
Product |
Storage |
File System |
Case-Sensitive |
---|---|---|---|
AKD PDMM PCMM PCMM2G |
Embedded Flash |
FFS3 (POSIX-like) |
Yes |
AKD PDMM PCMM |
SD card / USB flash drive |
FAT16 FAT32 |
No |
Example
- Two files (MyFile.txt and myfile.txt) can exist in the same directory of the controller's flash.
- They cannot exist in the same directory on the controller’s SD card.
- If you copy two files (via backup operation or function) with the same name but different upper/lower case letters, from the controller's flash to the SD card or USB flash drive, one of the files is lost.
-
- Use unique file names to prevent conflicts and to keep the application compatible across all platforms.
Do not rely on case-sensitive file names.
See Also