FatalStop
Function - Breaks the cycle and stop with fatal error.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
BOOL |
FALSE, TRUE |
|
|
Condition. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
BOOL |
FALSE, TRUE |
|
TRUE if performed. |
Remarks
- This function breaks the current cycle and sets the Virtual Machine in ERROR
mode.
- Restarting normal execution is performed using the debugger.
- The VM is stopped only if the IN argument is TRUE.
- The end of the current cycle is then not performed.
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
Not available.
See Also