MakeDWord
Function - Builds a double word as the concatenation of two words.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
HI |
USINT |
|
|
|
Highest significant word. |
|
LO |
USINT |
|
|
|
Lowest significant word. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
UINT |
|
|
32-bit register. |
Remarks
None
FBD Language Example
FFLD Language Example
- In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
- The function is executed only if EN is TRUE.
- ENO keeps the same value as EN.
IL Language Example
- In the IL Language, the input must be loaded in the current result before calling the function.
Op1: LD HI
MAKEDWORD LO
ST Q
ST Language Example
Q := MAKEDWORD (HI, LO);
See Also