not_mask
Function - Performs a bit-to-bit Boolean negation of an integer value.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
ANY |
|
|
|
Integer input. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
ANY |
|
|
Bit to bit negation of the input. |
Remarks
- Arguments can be signed or unsigned integers from 8- to 32-bits.
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung (EN) enables the operation.
- The output rung keeps the state of the input rung.
- The function is executed only if EN is TRUE.
- ENO has the same value as EN.
IL Language Example
- In the IL Language, the first parameter (IN) must be loaded in the current result before calling the function.
- The other input is the operands of the function.
Op1: LD IN
NOT_MASK
ST Q
ST Language Example
Q := NOT_MASK (IN);
See Also