ascii
Function - Get the ASCII code of a character within a string.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
STRING |
|
|
|
Input string. |
|
POS |
DINT |
|
|
|
Position of the character within the string. The first valid character position is 1. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
CODE |
DINT |
|
|
Either:
|
Remarks
None
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung (EN) enables the operation.
- The output rung (ENO) keeps the same value as the input rung.
IL Language Example
- In the IL Language, the first parameter (IN) must be loaded in the current result before calling the function.
- The other input is the operand of the function.
Op1: LD IN
AND_MASK MSK
ST CODE
ST Language Example
CODE := ASCII (IN, POS);
See Also