ESI and ENI Files
The EtherCAT master uses the information from the ENI file to initialize and configure the EtherCAT network.
- The ESI files are provided by the vendor for each device.
- They contain information about the device functionality and its settings.
- The ESI files are used by the KAS-IDE to generate the ENI file.
- The KAS controller’s EtherCAT master uses the ENI file for network initialization and configuration.
Figure 1: EtherCAT Network Architecture 1
-
-
KAS uses ENI schema version 1.3 (May 20, 2009).
See the ETG.2100 specification at www.ethercat.org for more information.