CAM Profile Switching

At pipe network start-up or when using the MLCamSwitch function block, a CAM block's output position is set to the output position of the initialized profile.

Assume

  • This profile is switched on.
  • The present pipe network position is:
    • 150 at the input of the CAM block.
    • 50 at the output of the CAM block.

Result

  • As the input to the CAM block increases or decreases, the CAM output value increases or decreases respectively.
  • It will go through the modulo without a position jump.