Create a KVB Project

KVB projects are managed in the Project Explorer.

Use this procedure to create a project:

  1. In the Project Explorer, right-click on the System item to open the contextual menu.
  2. Select the Add HMI device command.
  3. Select the device name within the list and click OK.

    Select an AKI

  4. Figure 1: Select an AKI to add.



    • The content varies depending the version of KVB installed on your system.
      If you have KVB 1.1 installed you may open projects that have a KVB 2.1 panel but you cannot open the panel in KVB.

  5. Right-click on the newly created item and select the Rename command to change its name.
  6. Right-click and select the Add KVB Project command.

  • This command is disabled when a KVB panel is already created for the current HMI device.

Concept Link IconSee Also