Create a PLCopen Axis
-
In the Project Explorer, under PLCopen, right-click the Axes folder and select the New Axis command in the menu.
-
Give the new axis a name the Create PLCopen Axis dialog.
- Fill in the axis properties by right-clicking on the new axis.
See Modify PLCopen Axis for details. -
Compile the project to generate the code for the PLCopen axis reference(s).Each axis will show in the variable type PLCopenCode, which is used by the PLCopen Global variable.
-
The PLCopen.XXXXXX_ref (MyAxis1 in the example below) is an instance of an AXIS_REF Structure that can be used in your PLC programs.
-
-
The PLCopen axis Name and Number in the PLCopen Axis Data dialog, are automatically applied to the PLCopen instance under Global variables in the Dictionary when the project is compiled.