Direct Method Connection
This method is used when SafePLC2 is installed on the same computer as the KAS-IDE.
The procedure assumes you have already added a SafePLC2 project to the KAS project tree (see Direct Method Connection).
- Double-click on the SafePLC2 node.
Alternatively, right-click on SafePLC2 and select Open SafePLC2.
- SafePLC2 and the Safety Project open.
SafePLC2 automatically populates the safety devices from the EtherCAT Safe topology defined in the KAS-IDE. - Complete and save the SafePLC2 Safety Project.
- Compile the Safety Project and download it to the SCU1 controller.
- Return to the KAS-IDE to complete and compile the project.
The KAS-IDE automatically creates the required black channel communication required for FSoE from the connected module information passed to the KAS-IDE from SafePLC2.
- Download the compiled KAS application to the controller and run it.
- The Black Channel will establish the Safety network connection when EtherCAT goes into the operational state.
- The SCU transitions to Run mode.
-
-
- The KAS project supports a single SafePLC2 instance and project.
- The SafePLC2 node cannot be deleted while the application is running.
- The KAS-IDE cannot be closed while SafePLC2 is running with a synchronized project.
See Also
AKD2G Safety Parametrization Using FSoE with SCU-1-EC and PxMM / PCMM2G