Compare PLC Programs
-
-
- Use the Compare Projects to compare project files.
- The function for comparing the local project file to that on the controller is accessed from a button on the Status Bar, between the Local and Controller versions.
- It is active when KAS is connected to a controller.

- It is active when KAS is connected to a controller.
Once files have been selected to compare, a window opens listing the components of each project and any differences between them.
- How the projects differ is color coded.
- Red item indicates where there is a mismatch.
- Double-click to open an item. The << button brings you back to the list.
Figure 1: Listing the Differences
This message appears if you click on the compare button but the project is not present on the controller.![]()
Limitations of FFLD Diagrams
If one or more components within a network differ, then the entire network is displayed in the diff view with a gray background.
Differences between individual components within the network are not specified in any way.
Example: Figure 2 has a comparison of two FFLD programs.
- Network #1 differs, but the actual difference is not called out or highlighted.
- The difference is the last element: a coil on the left diagram and an inverted coil on the right diagram.
- Network #2 is the same on the left and right, so it has a white background.