Booting the AKD PDMM or PCMM Controller

This topic explains the boot sequence for the controller, which is based on the RAM and the Flash memory.

The flash memory contains two images:

  • Recovery image (4 Mb) contains QNX operating system and the KAS web server.
  • Regular image (9 Mb) contains QNX operating system, the KAS web server, and the KAS Runtime.

See Also