Using SSH
The Kollmorgen controllers can be accessed using SSH.
- SSH is used to perform maintenance operations that are not available through the web interface.
- Kollmorgen Application Engineers may need to use SSH to access the controller to help resolve customer issues.
Login
- AKD PDMM and PCMM allows login using the root user.
- PCMM2G only allows access to the admin user.
Because the admin user is in the sudo group, the user can use root privileges to perform maintenance using the sudo command.
- Internally, the controller uses a kas user account.
- It is recommended to not use this account because files in the kas user directory are critical to the proper functioning of the controller.
-
-
To ensure security, it is critical that the login password be changed from the default value.
See Change Controller's Password using SSH for more information.
See Also