Help menu

Command

Description

Documentation

Opens the help system.

Help Preference

As stated in Is the Help System Online or Offline?, there is more than one type of help system with different advantages.

By default the Online version is used.

If you prefer, you may specify which Help version to use, the Online (default) or Offline (built-in) help system.

Kollmorgen Developer Network (KDN)

Opens a web browser to the Kollmorgen Developer Network (www.kollmorgen.com/developer-network/), a community support site.

About

Shows version numbers and other information about the KAS-IDE.

See also see "Find the KAS-IDE Version" on page 1.