AIN#.VALUE
Description
AIN#.VALUE reads the analog input value after the value is filtered (as shown in the Analog Input Block Diagram).
Examples
Code
--> AIN1.VALUE 1.420 V
Context
For more information see Analog Input.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | V |
| Range | -12.5V to +12.5V |
| Default Value | N/A |
| Data Type | Float |
| See Also | |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AIN1.VALUE |
3780h |
01h |
Signed16 |
- |
1000:1 |
Read only |
Yes |
|
AIN2.VALUE |
3781h |
01h |
Signed16 |
- |
1000:1 |
Read only |
Yes |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
23100 |
1 |
23100 (0x5a3c) |
AIN1.VALUE |
Signed16 |
Read Only |
Yes |
|
23101 |
1 |
23101 (0x5a3d) |
AIN2.VALUE |
Signed16 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AIN1.VALUE |
23100 |
Float |
Read Only |
- |
|
AIN2.VALUE |
23101 |
Float |
Read Only |
- |